AXIS#.FBUS.DEC

Description

This command allows reading the deceleration set by fieldbus when in certain fieldbus modes.

Fieldbus Applicable Modes
EtherCAT Profile position, Profile velocity
CAN Profile position, Profile velocity
PROFINET MDI_DEC signal, decel limit used when commanding velocity
EtherNet/IP Decel limit used for command types 6 (position move) and 7 (jog)

  • Writing to this command is possible and is used when AXIS#.CMDSOURCE is fieldbus. Depending on the fieldbus mode, may be overwritten by the fieldbus.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2 , (custom units)/s2

See Acceleration Units.

Range

Depends on units. See Acceleration Units.

Default Value

10,000 RPM/s

Data Type

Float

Stored in Non-Volatile Memory

Yes

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5101

1

5101 (0x13ed)

AXIS1.FBUS.DEC

Unsigned32

Read/Write

Yes

70637

2

5101 (0x13ed)

AXIS2.FBUS.DEC

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.DEC

5101

Float

Read/Write

Acceleration

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC